K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field

跳至解决方案
1,469 次查看
larryhartman
Contributor I

I see a note that this field has a write 0 to clear.   Is this a type, the convention used up to this point in the resource manual is to use write 1 to clear.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,421 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Larry:

That is not a typo, you have to write 0 to clear. This applies for both: [CF] and [ERR] bit fields.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,422 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Larry:

That is not a typo, you have to write 0 to clear. This applies for both: [CF] and [ERR] bit fields.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复