K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K20 Resource Manual--PDB Channel n Status Register (PDBx_CHS), CF field

ソリューションへジャンプ
1,482件の閲覧回数
larryhartman
Contributor I

I see a note that this field has a write 0 to clear.   Is this a type, the convention used up to this point in the resource manual is to use write 1 to clear.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,434件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Larry:

That is not a typo, you have to write 0 to clear. This applies for both: [CF] and [ERR] bit fields.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,435件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Larry:

That is not a typo, you have to write 0 to clear. This applies for both: [CF] and [ERR] bit fields.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信