K20 Reset bit Lockup set after sector erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K20 Reset bit Lockup set after sector erase

1,318 Views
degry
Contributor I

When I do Program Flash Sector Erase, bit1 (Lockup) in the RCM bloc is set. This means that the ARM core stops executing instructions.

 

First I initialize the flash bloc by calling FTFL_Initialization(); as defined defined in flash_kinetis.c.

 

Then I send one or more:

 

FTFL_EraseSector(0x0000A000);  // 0x0000A0000 can be different adresses of course...

 

The Lockup Reset happens sometimes after sending the 1st FTFL_EraseSector command, but mostly it happens after the 2nd. It seems to happen less if I wait very long after each erase cmd (>5s) (while debugging, single step), but that is not usable of course.

The flash sector is erased apparently before the lockup, but the processor hangs.

 

I use CW V10.2 + JLINK with a K20DX128.

 

Any idea? 

0 Kudos
Reply
1 Reply

909 Views
konrada
Contributor IV

I had spurious flashing errors which went away when I moved the flash cache reset (a write to FMC_PFB01CR) to the helper function which always runs from RAM. 

 

Related to your problem?

0 Kudos
Reply