K20 RTC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K20 RTC

2,062 次查看
vanajagujjala
Contributor III

Hello,

          I have a doubt on RTC,without external 32KHZ oscillator can we run the RTC in MK20DX128VLH5?Is there any other option to RTC wothout external 32KHZ oscillator.

any body please help me urgently.

Thanks

vanaja

标签 (1)
0 项奖励
回复
3 回复数

1,906 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Earl Goodrich II comments is quite correct.

The RTC module needs external 32.768KHz clock as clock source to keep RTC module keeping working with VBAT power supply.

Wish it helps.


Have a great day,
best regards,

Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,906 次查看
vanajagujjala
Contributor III

Thanks for the Reply.

Thanks,

vanaja.

0 项奖励
回复

1,906 次查看
egoodii
Senior Contributor III

You don't really say what you want to use the RTC registers FOR.  If you want any kind of timekeeping accuracy, or operation from battery while the rest of the CPU is 'off', then using the 32KHz input is indeed going to be necessary, whether that be a crystal or as a precision 32KHz oscillator input.

0 项奖励
回复