K20 PWM Unexpected Duty Cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K20 PWM Unexpected Duty Cycle

8,334件の閲覧回数
myke_predko
Senior Contributor III

I am trying to generate a 38kHz square wave using the MK20DN512VLL10's FTM0 module running under MQX (I don't think MQX would make any difference).  The purpose of this is to send out a modulated IR signal for object detection.  

The code that I'm using is (and was validated in AN5142 as well as a number of posts on the community forum here):

// Enable Flex Timer Clock
  SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;

  FTM0_SC = 0; // Make sure FTM0 is off before writing to it
  FTM0_MODE |= FTM_MODE_WPDIS_MASK; /* Disable write protection */
  FTM0_MODE |= FTM_MODE_FTMEN_MASK;
  FTM0_CONF |= FTM_CONF_BDMMODE(3); // counter run in BDM mode
  FTM0_CNTIN = 0x00;

  FTM0_CNT = 0; // Reset Counter
  FTM0_MOD = 48000000 / 38000; // Set PWM frequency; MODULO = Fclk/Fpwm

  FTM0_C7SC |= FTM_CnSC_MSB_MASK;  //  Set FTM0 Channel 7 Operation
  FTM0_C7SC |= FTM_CnSC_ELSB_MASK;
  FTM0_C7SC &= ~FTM_CnSC_ELSA_MASK;

  FTM0_C7V = FTM0_MOD / 2; // THIS SHOULD BE A 50% duty Cycle

//  Status and Control bits
  FTM0_SC = FTM_SC_CLKS(1) | FTM_SC_PS(0);

  PORTD_PCR7 |= PORT_PCR_MUX(4) | PORT_PCR_DSE_MASK; // FTM0 CH7 - high power operation

The PWM period is perfect but the duty cycle is above 77% (Period is 26.4us and the High part of the signal is 20.4us).   

I'm taking the period value and dividing it by two - anybody see where my problem is?  

Thanx,

myke

ラベル(2)
タグ(3)
0 件の賞賛
返信
18 返答(返信)

7,830件の閲覧回数
myke_predko
Senior Contributor III

Here's another data point:

I tried manually setting the compare value (FTM0_C7V) and discovered that the change in terms of the PWM isn't linear.  The timing values (measured on an oscilloscope) I got are:

FTM0_C7VPeriod (us)PWM High (us)PWM Low (us)C7V / PWM High
63126.420.46.00.032330
30026.413.612.80.045333
27526.413.213.20.048000
25026.412.4140.049600

It looks like the PWM counter/Compare module (FTM0_C7V & "output modes logic") is getting a different clock from the "FTM counter" and the "FTM0_MOD" register.  This doesn't make any sense when I look at the FTM block diagram (Figure 38-1) in the K20P100M100SF2V2RM (Reference Manual) documentation - I'm looking at Rev. 2 Jun 2012 which is the current at NXP.com.  

Any ideas what's going on here?  In the short term, I know what gives me a 50% duty cycle (FTM0_C7V = 275) but this doesn't make sense according to the documentation, other posts and example code.  

0 件の賞賛
返信

7,830件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi myke,

Have you try to observe the register value during debug in CodeWarrior11?
For example:FTM0_C7V and FTM0_MOD and FTM0_C7SC

Seems you have select EPWM:

Edge-Aligned PWM.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,830件の閲覧回数
venkateshgv
Contributor II

Hai,

 Am using  MC9S08SG8 micro controller ,and am using code warrior V6.3  software ,here am using PWM in 7th pin ,

 my problem is in  output duty cycle  first pulse is grater then the other pulse ,like this. plz any one can help me.Capture.PNG

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Hi Robin,

Thank you for the reply.  Yes, I am verifying the register values using CW. 

I did use that table from the Reference Manual for setting up the PWM and the bits you highlighted have been set with the three lines:

  FTM0_C7SC |= FTM_CnSC_MSB_MASK;  //  Set FTM0 Channel 7 Operation
  FTM0_C7SC |= FTM_CnSC_ELSB_MASK;
  FTM0_C7SC &= ~FTM_CnSC_ELSA_MASK;

When I check the FTM0_C7SC register in CW, I see the MS7B = 1, ELS7B = 1 & ELS7A = 0.  

Thanx again.  

0 件の賞賛
返信

7,830件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

The easiest way to get a 50% duty cycle is to choose Output Compare mode and configure it Toggle Output on match.
Please try to use this mode first.

37.4.5 Output Compare mode.png

Output Compare Toggle Output on match.png

You'd better to give me the register value screen capture, so that I can check if the register of FTM is correct or not.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Hey Robin,

Sorry for taking a few days to reply - I had a busy weekend and start to the new week (and I'm not even celebrating Thanksgiving).  

As requested, here are the register values, taken as screen shots from CW 11:

Let's start with FTM0_COMBINE (which includes DECAPEN# & COMBINE):

2018.11.27 - FTMO_COMBINE After Initialization.png

- DECAPEN# - All Bits Reset

- COMBINE# - All Bits Reset

Now, the documentation says that this is for "n = 6" - do I want for "n = 7" as I'm using FTM0_C7?

For FTMO_SC:

2018.11.27 - FTMO_SC After Initialization.png

- Bit 5 CPWMS (Center-Aligned PWM Select) - Reset which is what we want

Next is FTMO_C7SC:

2018.11.27 - FTMO_C7SC After Initialization.png

Using the datasheet:

Bit 5 - MSB (Channel Mode Select) - Set which is what we want

Bit 4 - MSA (Channel Mode Select) - Reset as it is a don't care for this application of the FTM

Bit 3 - ELSB (Edge or Level Select) - Set which is what we want

Bit 2 - ELSA (Edge or Level Select) - Reset which what we want for this application (ELSB:ELSA = 1:0 is "Clear Output on Match)

Any comments?  Other than the DECAPEN/COMBINE confusion regarding using them for FTMO_C7, I think I'm good.  

myke

0 件の賞賛
返信

7,830件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

If you want to get 50% duty PWM when FTM0_MOD=0x4ef, you should configure FTM0_C7V=0x277

FTM0_C7V.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Hi Robin,

Totally agree with what you're saying but...

When I run with the original values with the register set up and manually writing in 0x113:

2018.11.28 - FTM0_COMBINE Register.png

2018.11.28 - FTM0 Registers - 275.png

2018.11.28 - FTM0_C7 Registers - 275.png

I get the waveform:

2018.11.28 - FTM0_C7 Output - 275.jpg

Now, when I put in the expected 50% duty cycle value (0x277 as you noted) with the registers:

2018.11.28 - FTM0 Registers - MOD div 2.png

2018.11.28 - FTM0_C7 Registers - MOD div 2.png

I get the waveform:

2018.11.28 - FTM0_C7 Output - MOD div 2.jpg

I'm sure there's something that I'm doing wrong, but for the life of me, I can't figure out what it is.

Any ideas?

myke

0 件の賞賛
返信

7,830件の閲覧回数
mjbcswitzerland
Specialist V

Hi Myke

I just set up a uTasker project on a K20, running at 96MHz (as yours, with 48MHz bus clock):

    PWM_INTERRUPT_SETUP pwm_setup;
    pwm_setup.int_type = PWM_INTERRUPT;
    pwm_setup.int_handler = 0;
    pwm_setup.pwm_mode = (PWM_SYS_CLK | PWM_PRESCALER_1 | PWM_EDGE_ALIGNED); // clock PWM timer from the system clock with /1 pre-scaler
    pwm_setup.int_handler = 0;                                          // no user interrupt call-back on PWM cycle
    pwm_setup.pwm_reference = (_TIMER_0 | 7);                           // timer module 0, channel 7
    pwm_setup.pwm_frequency = PWM_FREQUENCY(38000, 1);                  // generate 1000Hz on PWM output
    pwm_setup.pwm_value   = _PWM_PERCENT(50, pwm_setup.pwm_frequency);  // 50% PWM (high/low)
    fnConfigureInterrupt((void *)&pwm_setup);                           // enter configuration for PWM test on PTD7
‍‍‍‍‍‍‍‍‍

I measured then 38kHz on PTD7 and 50% mark-space.

These are all the FTM0 registers

pastedImage_1.png

(I also had an output on channel 2 but ignore that).

I notice you have a very slow falling edge on your output but it my be due to loading you have.

I don't know whether it helps in any way but the setting above give the expected output.

Regards

Mark

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Hi Mark,

Thank you for your reply.  

Here are my registers:

2018.11.29 - FTM0 Register Values 1.png

2018.11.29 - FTM0 Register Values 2.png

2018.11.29 - FTM0 Register Values 3.png

2018.11.29 - FTM0 Register Values 4.png2018.11.29 - FTM0 Register Values 5.png2018.11.29 - FTM0 Register Values 6.png2018.11.29 - FTM0 Register Values 7.png

The differences between your values and mine are listed in the table below:

RegisterMark ValueMyke ValueComments
FTM0_MOD0x4EE0x4EFFTM Count Register/No issue
FTM0_C2SC0xA8FTM0_C4SC/FTM0_C5SC: 0x28Comparing to my _C4SC & _C5SC which have not run yet
FTM0_STATUS0xA40xA0Mark's value indicates that Channel 2 has overflowed
FTM0_MODE45Myke has FTM Enable Active 

So, unless the FTM Enable bit affects things, I think I have exactly the same operating environment as you do - comments?  

Finally, I'm scoping at the anode of an IR LED which is driven by a variable current supply, so the rounded edges when the signal goes low isn't that much of a surprise.  

Thanx for the comparison point - maybe something will come of it!

myke

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Nobody has commented in a while.  Anybody with any ideas?

Thanx!

0 件の賞賛
返信

7,830件の閲覧回数
mjbcswitzerland
Specialist V

Myke

FTM EN just allows the extended mode registers (those that the FlexTimer has but the TPM doesn't) to be used and shouldn't have any effect for basic PWM operation.

I have used the TPM and Flex Timers on most Kinetis part  and can't reproduce your problem so I am wondering whether it is coming from another part of the system or due to some measurement strangeness (?)

If you do need it solved I offer a professional service via Remote Desktop. There is a 40 minute free session which would probably do it, so there wouldn't be any complications with having to find funding. If you prefer directly at NXP they also do a service where you can trial direct support for 2 hours for $500.-

Regards

Mark


http://www.utasker.com/services.html

0 件の賞賛
返信

7,829件の閲覧回数
myke_predko
Senior Contributor III

Hi Mark, 

Have you worked with the MK20DN512VLL10 and its FTM0?  I'm wondering if this is a peculiarity of the part because what I'm seeing doesn't make sense (and it doesn't matter where I probe it).  

I will kick this back to my FAE and see if NXP has any ideas.

Thanx,

myke

0 件の賞賛
返信

7,830件の閲覧回数
mjbcswitzerland
Specialist V

Hi Myke

I specifically tested on a K20FX512VLQ12 and a K60DN512VMD10, whereby both should be equivalent to your part with regards to FTM0 and clocks, with the second essentially identical if Ethernet is not used.

If you tell me your clock source (oscillator or crystal and which crystal loading) and the pin your FTM0 output is on I can also give you a binary to try with on any part (unlike when using the NXP libraries I can build for any part without needing to port anything).

These are the mainstream boards that I have (plus I also have a lot of boards from industrial product developments which have some variations): http://www.utasker.com/kinetis.html

Regards

Mark

0 件の賞賛
返信

7,830件の閲覧回数
myke_predko
Senior Contributor III

Hi Mark,

I smiled at the phrase "should be equivalent".  I've been in this game to know that "should be" doesn't mean necessarily - I don't think either one of those components use the same die.   

Clock source is a Crystal 8MHz with 18pF caps and a 1M resistor.  The clocking mode is "High Gain".  Figure 26-4 of the Reference Manual shows the circuit used.  

Please send me your code and I'm going to try them on my TWR and Freedom boards (as well as with my code).  

Thanx,

myke

0 件の賞賛
返信

7,828件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the attached project.

38kHz PWM MK20DN512VLL10 CW10.7 PE.png

See also the registers value and the waveform of IR on TWR-K40D100M.

FTM0_CH7 PTD7 IR TWR-K40D100M.png

IR TWR-K40D100M.jpg

FTM0_CH7 PTD7 IR TWR-K40D100M waveform.bmp

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,827件の閲覧回数
mjbcswitzerland
Specialist V

Hi Myke

I have attached a binary file that I hope will run on the MK20DN512VLL10, driven by 8MHz crystal in high gain mode.
I configured for 96MHz PLL with 48MHz bus clock with a toggling output on PTC10 (pin 82) at 2.5Hz as a heat beat (to signal life).
There should be a 50% PWM signal on FTM0_CH7 (on PTD7 - pin 100). [FlexTimer clocked from bus clock with no pre-scaler to give the same values as you]
Since I don't have exact HW for this I simulated it only (see below) and the results look OK and your K20 matches closely to the 100 pin K60DN512 (which I set as major config).
Assuming that you can load a binary and it operates you can then check the output to see whether there is the unexpected mark-space or whether it is 50%.

Good luck

Regards

Mark

P.S: I don't know of any K20 tower or freedom board with your processor on.

P.P.S. I changed the attached file on 19.12.2018 at 17:16 because I had used the wrong linker script the first time....

pastedImage_1.png

0 件の賞賛
返信

7,827件の閲覧回数
myke_predko
Senior Contributor III

Additional data point.  

I *thought* that I could single step through the code (in "Instruction Stepping Mode") and see the FTM0_CNT register increment but this doesn't seem to work (I'm using a Segger debug tool and this is MQX 4.0.1 running in CW 11).  

Any other ideas as where I can look to understand what's happening?

0 件の賞賛
返信