K12 CRC-CCITT??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K12 CRC-CCITT??

1,584 Views
sywksmstkadlfgk
Contributor III

Someone use the CRC module of K12 ?

I'm using the CRC-CCITT Processor Expert settings but result don't match.

Testing with "123456789" the CRC is 0x6856 when the expected is 0x29B1..??

0 Kudos
Reply
1 Reply

1,364 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi  sywksms,

Please refer the answer in K12 CRC-CCITT .

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply