K10, multilink and SWD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10, multilink and SWD

1,506 Views
Alis5
Contributor I

Hello,

We have a product that have a Kinetis K10 processor in it.

We have programmed it by using PE-multilink and JTAG. We also have a small rig where we put our product and then have spring-pins/connectors connecting to some pads on the PCB. This has work pretty good (maybe 80% of the time). But now it's worse and worse (guessing that the rig is starting to get old, and the pins aren't that precise any more). So my thought was to program it through SWD instead, then it uses much less pins, (and then maybe get more stable).

But I have a hard time finding out how SWD works. It only says that "only 2 pins are needed". But I'm guessing that this is a truth with a modification. I suppose that gnd is needed as well. And how about reset and VCC, are they needed as well? How does SWD get in programming mode? JTAG does it when resetpin is still low (if I remember it correct), is it the same for SWD?

Has anyone tried to program a K10 with a multilink using SWD?

Is there anything else to change or should it work if it works to program it with JTAG (over multilink)? Just to check this SWD-box in the programming window?

0 Kudos
Reply
1 Reply

1,314 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check the <<Kinetis Peripheral Module Quick Reference>> page 35 Figure 2-8. 10-pin debug interface for SWD interface. Customer need to make sure the /EZP_CS pin is pull up or floating during chip reset.

Wish it helps.

0 Kudos
Reply