K10 UART3 Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 UART3 Question

1,827件の閲覧回数
keithkolmos
Contributor I


I have a K10 144 pin, 100Mhz design and I'm running into problems getting UART3 up and running properly

I have the clock gated to PORTE

SIM_SCGC5|= SIM_SCGC5_PORTE_MASK;   // to get Port E Clock enabled

and I have the clock gated over to PORTE

SIM_SCGC4 |= SIM_SCGC4_UART3_MASK;  // to get clock to the UART

And I have selected alternate function 3 for the RX and TX pins

PORTE_PCR24 = PORT_PCR_MUX(3);

PORTE_PCR25 = PORT_PCR_MUX(3);

I'm enabling UART3's IRQ (status vector)

enable_irq(51);

and I have the ISR function loaded into vector 67 in the vector table

I have UART 3 setup like this (I'm looking for 9600 baud, N,8,1)

    UART3_C2=0x00;

  UART3_BDH=0x00;

    UART3_BDL=0x89;

    UART3_C1=0x00;

    UART3_S2=0x00;

    UART3_C3=0x00;

    UART3_C2=0x2C;    

Just to double check things I have the UART RX and TX lines jumpered together on the output connector of my board so I should (in theory) see the data back on the receive buffer every time I transmit

But I'm never seeing any data on the TX pin and obviously not seeing the Receive Pin IRQ for getting any data back.

What am I missing?

Thanks for the help

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,686件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi, Keith Kolmos

You can generate a project according to the "Block reception/transmission, with interrupt service"  , the Typical Usage of Component Serial_LDD in CodeWarrior10.5 with PE.

Hope that help.

Best Regards

Binbin

0 件の賞賛
返信

1,686件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Keith Kolmos

From your code, you do not send out any data from TX, so you cannot find waveform from TX line. For register setting in your code is correct.

I suggest you to have a look at Freescale sample project on www.freescale.com There are many UART function operation for your reference.

Hope my reply can help you.

Best Regards

Paul

0 件の賞賛
返信