K10 QFN32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10 QFN32

1,777 Views
tahirmahmood
Contributor I

Hello,

Where should I connect the thermal pad of the K10 QFN 32 package. Should I connect it to ground plane because data sheet does not mention any thing. If I do not use both RTC and normal external oscillators and just use the internal clock then where should I connect these pins. Can I leave them unconnected? Is there any performance difference if I do not use external crystal oscillator?

BOWA-electronic GmbH & Co. KG

Tahir Mahmood

MSc.

Entwicklung Elektronik

BOWA-electronic GmbH & Co. KG

Heinrich-Hertz-Straße 4-10

D-72810 Gomaringen

Phone:

+49-7072-6002-925

Fax:

+49-7072-6002-3925

E-mail:

[email protected]<mailto:[email protected]>

Internet:

bowa.de<http://www.bowa.de/>

BOWA-electronic GmbH & Co. KG mit Sitz in 72810 Gomaringen

Geschäftsführer: Jens Kröber, Martin Heinrich

Registergericht: Stuttgart, HRA 381478

Umsatzsteuer ID Nr.: DE240259728

0 Kudos
Reply
1 Reply

1,494 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Tair

For the thermal pad please check the application note AN1902

For the pins the recomendation is For the Kinetis family it is recommended to leave unused pines floating and configure them as disabled.

Please also check the AN4470

Is there any performance difference if I do not use external crystal oscillator?

the difference is that with external oscillator you can have a more accurate clock frequency if you use a better oscilator than the internal clock, also in some configuration you will have a low power consumption

Regards

Vicente Gomez

0 Kudos
Reply