JTAG Chaining K10 with Xilinx Ultrascale FPGA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JTAG Chaining K10 with Xilinx Ultrascale FPGA

4,069 次查看
lalit_verma
Contributor II

Hi,

We are designing a VPX SBC board in which we are using K10 as IPMC. Now we have Xilinx FPGA also on the board.

Now, as per VPX standard connector, there is only one port of JTAG available on P0 connector.

So, we are planning to include Xilinx FPGA and K10 microcontroller in a single JTAG chain.

As, per Xilinx, Vivado can identify third part devices but need to import a csv file in Vivado which includes details like ID code etc:

 

My questions here are:

1. Does K10 IDE supports third party devices in the JTAG chain?

2. Please share the properties required for detecting K10 in Xilinx Vivado IDE like 

idcodemaskirlenname

 

I am attaching the example csv file required by Xilinx.

An early response will be highly appreciated.

 

Thanks,

Lalit

 

 

4 回复数

3,992 次查看
lalit_verma
Contributor II

Hi XiangJun Rong,

I can see that NXP supports PEmicro Multilink debuuger for K10.

Please find below the link which describes how we can do JTAG daisy chaining using Multilink with different devices like K10 MCU, FPGA etc:

https://www.pemicro.com/blog/index.cfm?post_id=136

Now, if there is an option for enabling JTAG daisy chaining in MCUXPresso, it will be really helpful for us.

Please let me know how to enable JTAG daisy chaining in MCUXPresso.

 

Thanks,

Lalit

0 项奖励
回复

3,957 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you pointed out that the probe devices such as J-Link and Multilink Universal support the JTAG daisy chain function, but the IDE such as MCUXPresso tools does not support the jtag daisy chain function.

BR

XiangJun Rong

0 项奖励
回复

4,014 次查看
lalit_verma
Contributor II

Hi NXP team,

 

Any response on this will he very helpful for us.

 

Thanks,

Lalit

0 项奖励
回复

3,998 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Lalit,

I suggest you use dedicated JTAG connector for both K10 and FPGA.

The JTAG chain requires IDE tools support for example Keil, MCUXPresso or IAR and the probe device support like Segger J-Link device, it is difficult.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复