JN5168 - Can't enter programming mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JN5168 - Can't enter programming mode

2,069件の閲覧回数
mchiri77
Contributor I

Hi everyone! I've bought a JN5168 module (JN5168-001-M00), with a USB to TTL adapter (3,3V). I have some trouble entering the programming mode. The BeyondStudio flash programmer doesn't recognized the chip, appearing the error "Failed to read chip details on COM3".

I've check the connections from the module to the adapter and they are correct (RX to TX and viceversa, SPIMISO to ground through a switch, the same with RESETN but including a pull up resistor and a capacitor)

Do you know where the problem can be? There is few information about the JN5168, and it seems that many people have problems with it.

Thanks for the help!!

1 返信

1,366件の閲覧回数
EarlOrlando
Senior Contributor II

Hello!

Thank you for your interest in NXP products.

We are happy to support you through our communities, unfortunately we temporarily have a community structure with two parallel systems which has probably not guided you correctly.

Be ensured we are working on fixing the navigation and the offering as soon as we can.

In the meantime, please re-post your question into the monitored space for this product line:

https://nxpcommunity.force.com/community/CommunityForumQuestionList?category=ZigBee

You may find the following page helpful for navigating to the right spaces:

http://www.nxp.com/support/communities:COMMUNITIES

We apologize for the inconvenience,

The NXP Technical Support Team

0 件の賞賛
返信