J199 labels are misleading on FRDM-K64F Quick Reference Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

J199 labels are misleading on FRDM-K64F Quick Reference Card

1,420件の閲覧回数
dougturnbow
Contributor I

FYI the pin labels are next to the wrong pins for J199 on the Quick Reference Card for the FRDM-K64F.

This is the red & white card that comes as part of the packaging for the Freedom board.

The J199 connector is shown in one image (Figure 1) with an arrow pointing to it from a label "Add-on BT Module JY-MCU BT Board V1.05"

The other image (Figure 2) shows labels for each pin (1-P3V3, 2-GND, 3-PTC14, 4-PTC15) but the label for pin 1 is next to pin 4 and vice-versa.

ラベル(1)
0 件の賞賛
返信
1 返信

1,234件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Doug:

You are right, the J199 header numbers are mirrored in that card. We apologize for this inconvenience, which could cause connection problems.

Thank you for your observation, I will communicate it to the proper marketing team.

Regards!

Jorge Gonzalez

0 件の賞賛
返信