Issues with FRDM-KE02Z board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with FRDM-KE02Z board

1,297件の閲覧回数
robinkwek
Contributor I

Hi,

I am using FRDM-KE02Z board and tried to toggle PTA2, PTA3 (using BitIO component in PE). However, there is no response from the pin (using an oscilloscope to monitor). Also, I have disconnect R45, R42 and connected R47 and R39. Other pins are working fine. I am using KDS with PE (Processors with MKE02Z64VQH4) connected via SWD.   Is there anything that i missed out in my settings and any history of this issue?

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
1 返信

1,214件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Robin Kwek,

Please notice that PTA2 and PTA3 are true open-drain pins when operated as output.

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信