Issues on Kinetis K40 - UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues on Kinetis K40 - UART

1,820 Views
abulhasan
Contributor I

Hi

     I am having KwikStik K40 device. In that we are communicating with the SIM module(SIM900A) through UART. The SIM module has RS232 port. And we have checked using MAX232 to transmit and receiving the signals. It can transmit and receive when we loop back the TXD and RXD signals in K40. But it fails to work if we connect it to the SIM module. Whether we want to use RS232 protocol or RS485 protocol. If it is RS485 what type of level translator to be used.

Thank you.

0 Kudos
Reply
2 Replies

1,574 Views
JimDon
Senior Contributor III
0 Kudos
Reply

1,574 Views
erikmalund
Contributor I

post a link to the datasheet for the SIM900A

Whether we want to use RS232 protocol or RS485 protocol. neither RS232 nor RS485 are protocols

If it is RS485 what type of level translator to be used. surprise! a RS485 transceiver

Erik

0 Kudos
Reply