Issue regarding error which appeared during erasing MKL26Z64VFT4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issue regarding error which appeared during erasing MKL26Z64VFT4

8,459件の閲覧回数
dileeptn
Contributor I

Hai , 
We faced an issue in jlink command when trying to mass erase MKL26Z64VFT4. I have mentioned the error below. 


Error: 

SEGGER J-Link Commander V6.33a (Compiled May 9 2018 17:23:00) 
DLL version V6.33a, compiled May 9 2018 17:22:41 

Connecting to J-Link via USB...O.K. 
Firmware: J-Link V9 compiled Apr 20 2018 16:47:26 
Hardware version: V9.30 
S/N: 269302709 
License(s): FlashBP, GDB 
OEM: SEGGER-EDU 
VTref=3.322V 


Type "connect" to establish a target connection, '?' for help 
J-Link>connect 
Please specify device / core. <Default>: MKL26Z64XXX4 
Type '?' for selection dialog 
Device>device mkl26z64xxx4 
Please specify target interface: 
J) JTAG (Default) 
S) SWD 
F) FINE 
I) ICSP 
C) C2 
TIF>s 
Specify target interface speed [kHz]. <Default>: 4000 kHz 
Speed>1000 kHz 
Device "MKL26Z64XXX4 (ALLOW SECURITY)" selected. 


Connecting to target via SWD 
InitTarget() 
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. 
For debugger connection the device needs to be unsecured. 
Note: Unsecuring will trigger a mass erase of the internal flash. 
Executing default behavior previously saved in the registry. 
Device will be unsecured now. 
Found SW-DP with ID 0x0BC11477 
AP map detection skipped. Manually configured AP map found. 
AP[0]: AHB-AP (IDR: Not set) 
AP[1]: CUSTOM-AP (IDR: Not set) 
AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00 
InitTarget() 
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. 
For debugger connection the device needs to be unsecured. 
Note: Unsecuring will trigger a mass erase of the internal flash. 
Executing default behavior previously saved in the registry. 
Device will be unsecured now. 
Found SW-DP with ID 0x0BC11477 
AP map detection skipped. Manually configured AP map found. 
AP[0]: AHB-AP (IDR: Not set) 
AP[1]: CUSTOM-AP (IDR: Not set) 
AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00 

****** Error: Could not find core in Coresight setup 
InitTarget() 
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. 
For debugger connection the device needs to be unsecured. 
Note: Unsecuring will trigger a mass erase of the internal flash. 
Executing default behavior previously saved in the registry. 
Device will be unsecured now. 
Found SW-DP with ID 0x0BC11477 
AP map detection skipped. Manually configured AP map found. 
AP[0]: AHB-AP (IDR: Not set) 
AP[1]: CUSTOM-AP (IDR: Not set) 
AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00 
InitTarget() 
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set. 
For debugger connection the device needs to be unsecured. 
Note: Unsecuring will trigger a mass erase of the internal flash. 
Executing default behavior previously saved in the registry. 
Device will be unsecured now. 
Found SW-DP with ID 0x0BC11477 
AP map detection skipped. Manually configured AP map found. 
AP[0]: AHB-AP (IDR: Not set) 
AP[1]: CUSTOM-AP (IDR: Not set) 
AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00 
Cannot connect to target. 

The above shown as mentioned above are the errors which were generated while trying to erase or unlock the IC. 
I am not able to do any operation to the MKL IC and cant even access it either. It shows errors as shown above. I tried most of the techniques to mass erase the IC but finally landed nowhere. When i searched in NXP for the solution of the errors.....i found a reply for one of the questions that the IC is brick and can't be used.What are your suggestions regarding this? If the IC is not Brick what could be the possible issue behind such an error?We are presently using samples which were provided as per our request from the NXP.Is there any other software we should try to unlock or erase the IC.Since the Project is so urgent please kindly help me with this issue.

any help will be appreciated......

ラベル(1)
0 件の賞賛
返信
1 返信

6,672件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Customer,

    This is the same question as your another post, please check that post, I already reply you:

Unable to unlock MKL26z64vft4 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信