Is this an MKL03Z8VFG4?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is this an MKL03Z8VFG4?

ソリューションへジャンプ
2,278件の閲覧回数
PeterK
Contributor III

Hello,

Just recently I ordered some MKL03Z8VFG4s from a distributor. Having arrived, and unpacking, I realized that I had been sent some ATMEL-something chips and I returned them. Now the replacement chips have arrived. I assume that they are the right ones this time, but want to make sure.

I Guess I lost a little confidence in the distributor.

Packaging is QFN-16 and the chips are quite small, 3mmx3mm. It SEEMS like the marking/mask is "M3T4AABJ". But I am not 100% sure. The device datasheet has no information on chip markings/masks. Likewise the family datasheet and the latest ERRATA (1N86k).

I just want to verify, that I got the right chips.

Any help would be appreciated.

Thanks,

  Peter K

1 解決策
2,055件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hi Peter,

I have just look at my MKL03Z8VFG4 samples and can confirm that size 3mmx3mm and M3T4AABJ marking are correct.

Martin M.

元の投稿で解決策を見る

2 返答(返信)
2,055件の閲覧回数
PeterK
Contributor III

Thank you for replying, Martin.

That solved my specific immediate need.

In general, I wonder where that information is kept.

Thanks again,

  Peter K

0 件の賞賛
返信
2,056件の閲覧回数
MarMi
NXP Employee
NXP Employee

Hi Peter,

I have just look at my MKL03Z8VFG4 samples and can confirm that size 3mmx3mm and M3T4AABJ marking are correct.

Martin M.