Is there are flash example for the K20?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there are flash example for the K20?

跳至解决方案
1,671 次查看
rhana
Contributor III

Hello,

   I am looking for a flash example for the k20 (specifically for TWR-K20D72M.)  Is it different than for the k60 or is writing to the flash the same for the kinetis family?

Thanks.

1 解答
1,301 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Robert:

If you installed CodeWarrior v10.6, there is a Flash example for your board using processor expert at the next path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M\FLASH

In case you do not like or simply don't want to use PEx, you can always download the C90TFS Driver from the next link:

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe

The package includes examples and instructions on how to use the flash APIs.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,301 次查看
mjbcswitzerland
Specialist V

Robert

Flash writing is identical for the K20D72 and K60 (without FPU).

The following gives some details Re: Re: Serial number programming in production - Kinetis K10 (towards end)

Generally the differences (valid for KE, KL and K parts) are:

- parts with FPU and KE parts use phrase programming (8 bytes at a time) and other parts use long word programming (4 bytes at a time)

- the sector size varies between 512 bytes (KE parts), 1k (KL parts and some slower K parts - <= 50MHz), 2k most other parts, and 4k for FPU parts

There is a Flash driver that supports (automatically adapts itself to) all KE, KL and K parts in kinetis.c at http://www.utasker.com/forum/index.php?topic=1721.0

Regards

Mark

1,302 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Robert:

If you installed CodeWarrior v10.6, there is a Flash example for your board using processor expert at the next path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\TWR-K20D72M\FLASH

In case you do not like or simply don't want to use PEx, you can always download the C90TFS Driver from the next link:

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe

The package includes examples and instructions on how to use the flash APIs.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复