Is there any register in K60 for switching between nand flash controller and flex bus interface?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any register in K60 for switching between nand flash controller and flex bus interface?

ソリューションへジャンプ
1,227件の閲覧回数
shabeenakm
Contributor I

hi, anyone please help me to solve this problem... urgent please

thanks in advance..

ラベル(1)
0 件の賞賛
返信
1 解決策
1,059件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

K60 100MHz does implement an arbitration scheme that allows for sharing between the FlexBus and NFC.

There is no related register to switch the NFC and Flexbus.

About Flexbus and NFC related pin setting, there with two situations:

1> this sharing is really only used for the NFC data lines/FlexBus AD lines and the NFC_WE and FlexBus R/W signals. If you look at the signal muxing table in the manual you can see that these pins only have a single function selection for FlexBus/NFC.  For example, PTB20 function ALT5 is “FB_AD31/NFC_DATA15.” So this is a case where the pin is configured for a FB/NFC mode and dynamically switches between the two.

In the case of the control signal pins that (NFC_CE0 and NFC_RB) the pins for these signals have different programmed functions to choose between the FlexBus and NFC signals on the pins. So for those signal the pin does not dynamically switch between the functions. It is fixed as a FlexBus or NFC pin based on whether you choose ALT5 or ALT6.

Wish it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,060件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

K60 100MHz does implement an arbitration scheme that allows for sharing between the FlexBus and NFC.

There is no related register to switch the NFC and Flexbus.

About Flexbus and NFC related pin setting, there with two situations:

1> this sharing is really only used for the NFC data lines/FlexBus AD lines and the NFC_WE and FlexBus R/W signals. If you look at the signal muxing table in the manual you can see that these pins only have a single function selection for FlexBus/NFC.  For example, PTB20 function ALT5 is “FB_AD31/NFC_DATA15.” So this is a case where the pin is configured for a FB/NFC mode and dynamically switches between the two.

In the case of the control signal pins that (NFC_CE0 and NFC_RB) the pins for these signals have different programmed functions to choose between the FlexBus and NFC signals on the pins. So for those signal the pin does not dynamically switch between the functions. It is fixed as a FlexBus or NFC pin based on whether you choose ALT5 or ALT6.

Wish it helps.

0 件の賞賛
返信
1,059件の閲覧回数
shabeenakm
Contributor I

Thank you bmwhui, It is helpful...

0 件の賞賛
返信