Is there any method to delete Program Flash IFR?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any method to delete Program Flash IFR?

1,521件の閲覧回数
aaronledger
Contributor I

I understand the purpose of the Program Flash IFR Program Once area is to be able to only write once to this non-volatile storage, but is there any way to initialize this memory via debugger? I have tried mass erasing the part (KW24) with no success as the IFR bytes I wrote persist.

0 件の賞賛
返信
1 返信

1,366件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

No, actuually this register can not been see & edit in memory map. Customer can only read the IFR values by the corresponding command.

0 件の賞賛
返信