Is there any method to delete Program Flash IFR?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any method to delete Program Flash IFR?

1,571 次查看
aaronledger
Contributor I

I understand the purpose of the Program Flash IFR Program Once area is to be able to only write once to this non-volatile storage, but is there any way to initialize this memory via debugger? I have tried mass erasing the part (KW24) with no success as the IFR bytes I wrote persist.

0 项奖励
回复
1 回复

1,416 次查看
miduo
NXP Employee
NXP Employee

Hi,

No, actuually this register can not been see & edit in memory map. Customer can only read the IFR values by the corresponding command.

0 项奖励
回复