Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

1,442 Views
randyfields
Contributor II

I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.  I now would like to create an application using the USER_RUN_SPEED command and cannot get the motor to turn.  Is there an example of creating a project for applications other than running a motion plan?

Tags (1)
0 Kudos
Reply
1 Reply

1,342 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Randy,

I appologize for the delay.

Pls post your questions to the following KMS community:

https://community.nxp.com/community/kinetis/kms

The engineer in KMS team will give you better reply.

BR

Xiangjun rong

0 Kudos
Reply