Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?

1,052 次查看
randyfields
Contributor II

I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.  I now would like to create an application using the USER_RUN_SPEED command and cannot get the motor to turn.  Is there an example of creating a project for applications other than running a motion plan?

标记 (1)
0 项奖励
回复
1 回复

952 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Randy,

I appologize for the delay.

Pls post your questions to the following KMS community:

https://community.nxp.com/community/kinetis/kms

The engineer in KMS team will give you better reply.

BR

Xiangjun rong

0 项奖励
回复