Is there an OpenOCD 0.9.0 config for the K64F?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an OpenOCD 0.9.0 config for the K64F?

1,252 Views
robotdad
Contributor I

I'm looking for a config file for the K64F board for OpenOCD 0.9.0. The only config I can find for this board is in the KDS IDE which uses OpenOCD 0.8. Any suggestions?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,093 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Marc,

Why do you want use OpenOCD 0.9 ? Do you want to use the "GDB OpenOCD" to debug ?

If yes, you need update the firmware of the board use the bin of "0226_k20dx128_k64f_0x5000.bin" .

Hope it helps

Alice

0 Kudos
Reply

1,093 Views
robotdad
Contributor I

Thanks, I will give this a try this week.

I want to use 0.9 to simplify things on my end. I am working on getting mcu debugging working in Visual Studio, most of the debug targets I have are all on 0.9. So far the K64F is the only one I've been working with that I can only find an 0.8 config for.

0 Kudos
Reply