Is there an App Note or software available for a K60 to program a KL14/15 through the SWD interface?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there an App Note or software available for a K60 to program a KL14/15 through the SWD interface?

1,836 次查看
Larry5335
Contributor IV

Does Freescale or a 3rd party have software to do this?

标签 (2)
标记 (2)
1 回复

1,685 次查看
albertchen
Contributor I

Flashing Steps:

1.Power on the K64 and KL43.

2.Push  SW1 button on K60, then K64 will flash an binary into KL43.

3.Before flashing, the led D5 on K64 board is on; led D5 will be off when finished flashing.

Related docs:

1.KL43 RM, K64 RM

2.ARM® Debug Interface Architecture Specification.

3.ARMv7m Architecture Reference Manual.

Software Resources:

Keil 5.1


for detailed infomation, please see the SWD Flash Tool_V1.0.pptx.

Code: swd_flash_kl43Freedom.zip