Is there a way to restore the demo app on the FRDM_K22F board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a way to restore the demo app on the FRDM_K22F board?

1,757 Views
marcohess
Contributor II

A binary would be fine, but source code of the demo app would be great!

0 Kudos
Reply
4 Replies

1,552 Views
carlos_chavez
NXP Employee
NXP Employee

Hi Marco,

Attached is the binary for the Out-of-the-Box demo application.  The source for it will be made available on the web within the next two weeks.

Best Regards,

Carlos

0 Kudos
Reply

1,552 Views
BrianShay
Contributor II

Thank you Carlos! I was looking for the exact same thing.

0 Kudos
Reply

1,552 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Marco,

The FRDM-K22F board demo application could be downloaded from below link:

Software Development Kit for Kinetis MCUs|Freescale

The SDK software includes demos at default installation path: C:\Freescale\KSDK_1.0.0\demos


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,552 Views
ajj
NXP Employee
NXP Employee

Hi Ma Hui,

I have a customer also looking for the original code programmed into the FRDM-K22F.  I have looked thru the demo code in KDS 1.0.0 and am not seeing it.  I have not load every code example but they all seem to be simpler than the original code.  Am I missing it?  If so, can you point to which example is preloaded?  Otherwise, do you know where the original source code is?

Thanks,

Andy

0 Kudos
Reply