Is there a USB HID for printers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a USB HID for printers?

2,438件の閲覧回数
neilporven
Senior Contributor I


Hi everyone,

I would like to be able to send commands to a printer via the USB.  Is there a USB HID driver for printers or

is the USB HID capable of handling printers?

If anyone has links of examples, please let me know.

Thanks,

Neil Porven

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,125件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello,

MQX 4.2 has Host Printer Class support included at: <MQX_4_2_PATH>\usb\host\source\classes\printer eventhough there is not example application available, however, you can give a look to this driver that was created for generic printers.

I hope this can help you!

Best Regards,

Isaac

2,125件の閲覧回数
neilporven
Senior Contributor I

Thank you Isaac.

0 件の賞賛
返信