Is there a OpenSDA Debug Firmware in TWR K70 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a OpenSDA Debug Firmware in TWR K70 ?

Jump to solution
2,350 Views
joelesco
Contributor III

Hi,

I was working on the FRDM Board until now. I'm using the K70 and when I try to interfacing (for exemple with P&E GDB server) I cannot find port available for OpenSDA.

I ask again a stupid question I suppose....

Thanks for your answer !

Labels (1)
0 Kudos
Reply
1 Solution
2,151 Views
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

View solution in original post

0 Kudos
Reply
5 Replies
2,152 Views
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

0 Kudos
Reply
2,151 Views
joelesco
Contributor III

Humm.. I have another question about OSJTAG ! When I use the Flash programmer in CW can I flash ".elf" and also ".hex" ?

Thanks again !

0 Kudos
Reply
2,151 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2,151 Views
joelesco
Contributor III

Everything is on IT ! It's a wealth of valuable resources ! Thanks for sharing your knowledge !

0 Kudos
Reply
2,151 Views
joelesco
Contributor III

Thanks Erich, so much things to know with debugger !

0 Kudos
Reply