Is there a OpenSDA Debug Firmware in TWR K70 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a OpenSDA Debug Firmware in TWR K70 ?

跳至解决方案
1,545 次查看
joelesco
Contributor III

Hi,

I was working on the FRDM Board until now. I'm using the K70 and when I try to interfacing (for exemple with P&E GDB server) I cannot find port available for OpenSDA.

I ask again a stupid question I suppose....

Thanks for your answer !

标签 (1)
0 项奖励
回复
1 解答
1,346 次查看
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,347 次查看
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

0 项奖励
回复
1,346 次查看
joelesco
Contributor III

Humm.. I have another question about OSJTAG ! When I use the Flash programmer in CW can I flash ".elf" and also ".hex" ?

Thanks again !

0 项奖励
回复
1,346 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1,346 次查看
joelesco
Contributor III

Everything is on IT ! It's a wealth of valuable resources ! Thanks for sharing your knowledge !

0 项奖励
回复
1,346 次查看
joelesco
Contributor III

Thanks Erich, so much things to know with debugger !

0 项奖励
回复