Is there a OpenSDA Debug Firmware in TWR K70 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a OpenSDA Debug Firmware in TWR K70 ?

ソリューションへジャンプ
2,428件の閲覧回数
joelesco
Contributor III

Hi,

I was working on the FRDM Board until now. I'm using the K70 and when I try to interfacing (for exemple with P&E GDB server) I cannot find port available for OpenSDA.

I ask again a stupid question I suppose....

Thanks for your answer !

ラベル(1)
0 件の賞賛
返信
1 解決策
2,229件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,230件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The debug interface on the TWR-K70(F120M) is not OpenSDA, it is OSJTAG (S08 based). OpenSDA does not run on it.

0 件の賞賛
返信
2,229件の閲覧回数
joelesco
Contributor III

Humm.. I have another question about OSJTAG ! When I use the Flash programmer in CW can I flash ".elf" and also ".hex" ?

Thanks again !

0 件の賞賛
返信
2,229件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
2,229件の閲覧回数
joelesco
Contributor III

Everything is on IT ! It's a wealth of valuable resources ! Thanks for sharing your knowledge !

0 件の賞賛
返信
2,229件の閲覧回数
joelesco
Contributor III

Thanks Erich, so much things to know with debugger !

0 件の賞賛
返信