Is there MMA8451Q example code for FRDM-KE06Z ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there MMA8451Q example code for FRDM-KE06Z ?

5,794件の閲覧回数
kentachang_melt
Contributor II

Hello,

I am interesting to MMA8451Q, and found a MMA8451Q example code for FRDM-KL25Z. I have a FRDM-KE06Z board, and hope to run the MMA8451Q example code. Is there example code ?

Best Regards,

Kenta

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

4,944件の閲覧回数
kentachang_melt
Contributor II

Hi David,

Thank you so much.

Best Regards,

Kenta

0 件の賞賛
返信

4,943件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Kenta,

I migrated the sample code that you can find here to the FRDM-KE06Z board.

The complete source code is written in the Kinetis Design Studio v3.2.0  in collaboration with the FreeMASTER  tool in order to visualize the acceleration data.

Please find the whole project attached to this response.

I hope you find it useful.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

4,943件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You can get FRDM-KE06Z MMA8451Q support at http://www.utasker.com/kinetis/FRDM-KE06Z.html

This works with all popular IDEs (KDS, CW, IAR, Keil, Atollic, Greenhills etc.) and also on any Freescale board (KL25, KL27 etc. KE, K, KV etc. with first or second generation I2C design) so never needs any porting.

It is an industrial quality solution in case of professional requirements, or for education and hobby use too for faster learning and highest reliability and performance.

Regards

Mark

I2C user's guide: http://www.utasker.com/docs/uTasker/uTaskerIIC.PDF

[1 on 1 support available in English, German and French if ever needed]

4,943件の閲覧回数
rinipatel
Contributor III

Hi,

Here is the MMA8451Q example for FRDM-KE06Z from CW V10.6 installation path:

C:\Freescale\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\Kinetis\FRDM-KE06Z\I2C_PWM

Hope it helps

-Rini

0 件の賞賛
返信

4,943件の閲覧回数
kentachang_melt
Contributor II

Hi Rini,

I Do import I2C-PWM project into my new project, and build it, and then debug it. But there is a problem, the CW 10.6 does not connect with FRDM-KE06Z by the U-MultiLink. please help ...

Best Regards,

Kenta

0 件の賞賛
返信

4,943件の閲覧回数
rinipatel
Contributor III

Hi Kenta,

Have you tried using OpenSDA debug interface? Just like all other freedom boards, FRDM-KE06Z already comes with OpenSDA USB MSD Bootloader. You can update the OpenSDA firmware and load the OpenSDA debug application. And then select OpenSDA debug configuration in CW when you launch the code.

Regards,

Rini

0 件の賞賛
返信

4,943件の閲覧回数
kentachang_melt
Contributor II

Hello Rini,

I don't use OpenSDA debug interface, because I can use U-Multilink debug interface to run the I2C-PWM example project.

Thanks for your supports. 

Regards,

Kenta

0 件の賞賛
返信