Is it possible to emulate EEPROM using the P-flash of KE microcontroller?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to emulate EEPROM using the P-flash of KE microcontroller?

2,978 Views
simonefantuzzi
Contributor II

I see the microcontroller KE we have choose doesn't have EEPROM.

Is it possible to emulate it using a part of the 8kb flash?

Flex memory is not mentioned on the KE data sheet.

Thank you very much

5 Replies

2,557 Views
jmartinez1
Contributor II

Hi Carlos,

Thanks!

0 Kudos
Reply

2,556 Views
carlos_chavez
NXP Employee
NXP Employee

2,556 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Simone:

You may take a look to the application note "AN4903 EEPROM Emulation Driver for the Kinetis E Series Microcontrollers":

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4903.pdf

The appnote comes with a software package. To download it run a search in Freescale webpage for AN4903 and you will find it as a ZIP file:

pastedImage_7.png


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,556 Views
jmartinez1
Contributor II

Hi Jorge,

I want to use the flash as an EEPROM with MKE04 and I am interested in AN4903SW driver, which I can't found it. Please, can you send me the dowload link or zip?

Thanks.

Joaquim.

0 Kudos
Reply

2,556 Views
mjbcswitzerland
Specialist V

Hi Simone

I think that the following thread has the answer to your question:

https://community.freescale.com/message/482382#482382

Of course the 8k Flash is quite small but it is still possible to use a 512 byte sector to save parameters in (even if not pure EEPROM).

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support / µTasker FRDM-KE02Z40M support / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply