Is it possible to clock USB module with IRC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to clock USB module with IRC?

ソリューションへジャンプ
3,021件の閲覧回数
allankliu
Contributor III

Recently I am considering to design a macro USB dongle for Android (as HID/CDC device). Due to its limited space, I am trying to find a USB micro which can operate without external crystal. I know Microchip/Cypress can do, but STM claims that USB has to work with external crystal.

Can I use IRC(4MHz) of KL24/25Z as clock source for USB OTG?

Allan

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,806件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

It is impossible to use IRC for USB module because the internal reference clock does not have required accuracy which is strictly needed for peripheral USB.

Regard

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,806件の閲覧回数
egoodii
Senior Contributor III

For just CDC, the CP2105 is a tiny self-contained UBS-to-serial device.  Smaller & cheaper than an osc.

0 件の賞賛
返信
2,807件の閲覧回数
pavel_krenek
NXP Employee
NXP Employee

It is impossible to use IRC for USB module because the internal reference clock does not have required accuracy which is strictly needed for peripheral USB.

Regard

Pavel

0 件の賞賛
返信
2,806件の閲覧回数
DerekLau
Contributor IV

It's not recommended to use internal clock for USB applications.