Is it possible to Flash KEA8 uC series with st-link V2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to Flash KEA8 uC series with st-link V2?

1,400 Views
Vonsush
Contributor I

Is it possible to Flash S9KEAZN8amf uC with ST-link? If yes please share the steps to follow

I have used 20pin to 10pin adapter and connect to  ST-link V2. Below signals are connect to 20pin connector

Vcc, GND, SDIO, SCLK, Reset (used pull up). when connected drawing around 20mA of current .

 

0 Kudos
Reply
3 Replies

1,340 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Frankly speaking, the ST-LINK device is from ST, it can debug ST mcu, but I do not know if the ST-LINK can debug KEA family.

https://www.st.com/en/development-tools/st-link-server.html

You can use Multilink universal device from third party www.pemicro.com to download/debug KEA family.

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/automotive-mcus/ul...

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

1,335 Views
Vonsush
Contributor I

Thanks xiangjun

What about the J-Link Segger? Is it is possible to Flash KEA8 uC series with J-Link Segger in SWD mode?

0 Kudos
Reply

1,315 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the KEA family supports J-Link device in SWD mode.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply