Is fADCK (ADC conversion clock frequency) referring to the ADC clock source before it is being divided down? I'm assuming its after. But if so, doesn't the "Typical conversion time" example in 23.5.4.6.2 not meet the minimum since 8 MHz/8 = 1 MHz?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is fADCK (ADC conversion clock frequency) referring to the ADC clock source before it is being divided down? I'm assuming its after. But if so, doesn't the "Typical conversion time" example in 23.5.4.6.2 not meet the minimum since 8 MHz/8 = 1 MHz?

2,001 次查看
aarond1
Contributor I

Document Number: KL17P64M48SF6RM

16 bit SE output mode

0 项奖励
回复
3 回复数

1,718 次查看
EdgarLomeli
NXP Employee
NXP Employee

Hello Aaron.

ADCK signal is taken after the clock divider module as shown below:

ADCK signal.PNG

The complete block diagram is in 23.2.2

I think the example 23.5.4.6.2 it's wrong, the total conversion time it's:

ConversionTime = SFCAdder+AverageNum(BCT+LSTAdder+HSCAdder)

ConversionTime = (3ADCK+5BusK)+32(34ADCK+20ADCK)

ConversionTime = (3/1MHz +5/8MHz)+32(54/1MHz)

ConversionTime =1.731ms

Regards.

0 项奖励
回复

1,718 次查看
aarond1
Contributor I

But doesn't 1 MHz not meet the minimum operating condition for a 16 bit mode conversion as you can see from Table 27 in the datasheet?

pastedImage_1.png

0 项奖励
回复

1,718 次查看
EdgarLomeli
NXP Employee
NXP Employee

Hi Aaron. 

Unfortunately seems 23.5.4.6.2 example it's only for explanation purpose and does not considerate real operating conditions for the module. If you followed 23.5.4.6.2 configuration, an unexpected behavior would happen. 

Regards. 

0 项奖励
回复