Is bit-banding possible on the Kinetis? Any examples?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is bit-banding possible on the Kinetis? Any examples?

Jump to solution
3,389 Views
markosiponen
Contributor III

Is bit-banding possible on the Kinetis? Any examples?

I read here: https://en.wikipedia.org/wiki/ARM_Cortex-M that bit-banding is optional on the Cortex M0+.

0 Kudos
Reply
1 Solution
1,888 Views
antonioconcio
NXP Employee
NXP Employee

Hi,

You are right, it is optional and so bit-banding was not implemented in Kinetis-L because we have Bit Manipulation Engine (BME) which is much more powerful compared to bit-banding. You can find a chapter about it on each Kinetis L Reference Manual.

We have some examples in KL05/KL25 sample code, you can also refer to this THREAD.

Regards,

Antonio

View solution in original post

0 Kudos
Reply
3 Replies
1,888 Views
egoodii
Senior Contributor III

Specific 'Bit Banding', as per that ARM document, IS enabled in (at least) the Kinetis 'K' M4 devices.  Pretty easy to use on peripherals; there is even a macro for it in the Kinetis headers as 'BITBAND_REG'.  It is a little harder to use in RAM, mostly because the tools (compilers and linkers) won't help!  But here is an example for a graphics display RAM, in this case using the least-significant-byte of each 32-bit word as screen data (so that the upper bits can be preset for a SPI DMA refresh).

So, you have to pre-allocate the space yourself (fixed location, subtracted from the linker-space):

#pragma location=0x2000EF00

__no_init u32_t    Display_RAM[Y_PITCH*8];     //Pre-allocated fixed-space for Display RAM

                                     //Necessary, in SRAM-U, to use bit-banding!

Then the SRAM bit-band macro is pretty similar to theirs:

#define BITBAND_SRAM_A(Addr,Bit) (0x22000000u + (((u32_t)(Addr) - (u32_t)0x20000000u)<<5) + (((u32_t)(Bit))<<2))

and here is a line-drawing process using that bit-banding to avoid detailed RMW of display RAM bits, preferring instead to just write each single bit

///Draw a line from (xstrt,ystrt) to (xfin,yfin) using 32bit dashing 'pattern'

// modified Bresenham algorithm, using ARM M4 'bit banding' RAM access to allow direct bit-writes (no RMW)

#define Y_PITCH 132

void OLED_Line(u16_t xstrt, u16_t ystrt, u16_t xfin, u16_t yfin, u32_t pattern)

{

  s32_t eterm=0;       //Error-term from fractional accumulations

             ///Some kind of 'set to half' should improve centering the steps

  u16_t length;        //# of dots to draw

  s32_t diffx=xfin-xstrt;

  s32_t diffy=yfin-ystrt;

  u32_t _PTR_ offset;

  s16_t stepx=1<<5;   //Byte increment point for bit-band address

  u16_t ybit;

  if( xstrt > 127) xstrt = 127;              //A little sanity checking!

  if( xfin > 127) xfin = 127;

  if( ystrt > 63) ystrt = 63;

  if( yfin > 63) yfin = 63;

  ybit = ystrt&7;

  offset = &Display_RAM[xstrt];

  offset += (ystrt>>3)*Y_PITCH;         //8 bits of pixels per page, so add the page offset

  offset = (u32_t _PTR_)BITBAND_SRAM_A(offset,ybit);  //Convert to bit-band address, adding-in bit offset within byte for pixel row

  diffx=xfin-xstrt;

  diffy=yfin-ystrt;

  if (diffx<0)

  {

     stepx=-stepx;

     diffx=-diffx;

  }

  if (diffy<0)

  {

     diffy=-diffy;

      if (diffx>diffy)    //'mostly horizontal', move integer x, fractional y

      {

         length=diffx+1;

  //       eterm = diffy/2;

         for (u16_t i=0;i<length;i++)

         {

           register u32_t tmp;

           *offset=pattern;   //LSB-only is written

           tmp = (pattern&1)<<31;         //Compiler is SMART -- makes a proper ROR out of this pair!!!

           pattern = (pattern>>1) | tmp;

           offset+=stepx;

           eterm+=diffy;

           if (eterm>diffx)

           {

             eterm-=diffx;

             offset-=1;//<<2;       //Each step in y moves to the next bit, BUT once we underflow the byte

             ybit = (ybit-1)&7;         // where bitcount in bitband address is *4

             if(ybit == 7)                   // we must move to the LSB or MSB of the next row up/down.

                 offset -= (Y_PITCH<<5)-(8);//<<2);   //To next bitband byte location, less the 8-bit-count already done

           }

         }

      }

      else             //'mostly vertical', move integer y, fractional x

      {

         length=diffy+1;

  //       eterm = diffx/2;

         for (u16_t i=0;i<length;i++)

         {

           register u32_t tmp;

           *offset=pattern;   //LSB-only is written

           tmp = (pattern&1)<<31;

           pattern = (pattern>>1) | tmp;

           offset-=1;//<<2;       //Each step in y moves to the next bit, BUT once we underflow the byte

           ybit = (ybit-1)&7;         // where bitcount in bitband address is *4

           if(ybit == 7)                   // we must move to the LSB or MSB of the next row up/down.

               offset -= (Y_PITCH<<5)-(8);//<<2);   //To next bitband byte location, less the 8-bit-count already done

           eterm+=diffx;

           if (eterm>diffy)

           {

             eterm-=diffy;

             offset+=stepx;

           }

         }

      }

  }else

  { //Positive Y-direction:

      if (diffx>diffy)    //'mostly horizontal', move integer x, fractional y

      {

         length=diffx+1;

  //       eterm = diffy/2;

         for (u16_t i=0;i<length;i++)

         {

           register u32_t tmp;

           *offset=pattern;   //LSB-only is written

           tmp = (pattern&1)<<31;

           pattern = (pattern>>1) | tmp;

           offset+=stepx;

           eterm+=diffy;

           if (eterm>diffx)

           {

             eterm-=diffx;

             // Note: bitcount in bitband address is *4, but since 'offset' is a u32 pointer, this is accounted for

             offset+=1;//<<2;       //Each step in y moves to the next bit, BUT once we overflow the byte

             ybit = (ybit+1)&7;

             if(ybit == 0)                   // we must move to the LSB or MSB of the next row up/down.

                 offset += (Y_PITCH<<5)-(8);//<<2);   //To next bitband byte location, less the 8-bit-count already done

           }

         }

      }

      else             //'mostly vertical', move integer y, fractional x

      {

         length=diffy+1;

  //       eterm = diffx/2;

         for (u16_t i=0;i<length;i++)

         {

           register u32_t tmp;

           *offset=pattern;   //LSB-only is written

           tmp = (pattern&1)<<31;

           pattern = (pattern>>1) | tmp;     //Rotate-right 1

           offset+=1;//<<2;       //Each step in y moves to the next bit, BUT once we overflow the byte

           ybit = (ybit+1)&7;         // where bitcount in bitband address is *4

           if(ybit == 0)                   // we must move to the LSB or MSB of the next row up/down.

             offset += (Y_PITCH<<5)-(8);//<<2);   //To next bitband byte location, less the 8-bit-count already done

           eterm+=diffx;

           if (eterm>diffy)

           {

             eterm-=diffy;

             offset+=stepx;

           }

         }

      }

  }

}

0 Kudos
Reply
1,889 Views
antonioconcio
NXP Employee
NXP Employee

Hi,

You are right, it is optional and so bit-banding was not implemented in Kinetis-L because we have Bit Manipulation Engine (BME) which is much more powerful compared to bit-banding. You can find a chapter about it on each Kinetis L Reference Manual.

We have some examples in KL05/KL25 sample code, you can also refer to this THREAD.

Regards,

Antonio

0 Kudos
Reply
1,888 Views
markosiponen
Contributor III

Thank you. I also downloaded the  FRDM-KL25Z and TWRKL25Z48M Sample Code Package and looked at the BME examples.

0 Kudos
Reply