Is P-flash swap feature(Systems using flash memory swap) available in K20P100M72SF1 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is P-flash swap feature(Systems using flash memory swap) available in K20P100M72SF1 ?

1,193 Views
sudhanshubhutan
Contributor I

I need to support Robust Firmware upgrade using this feature, which K20 shall i select?

I read from product documentation, that 100MHZ variant supports this swap feature, its part

K20P100M100SF2V2  ?

Am i correct?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,120 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Sudhanshu Bhutani:

Just to clarify, you mentioned datasheet document numbers and not device part numbers.

About P-Flash swap:

- The existing K20_72 MHz parts do not have such feature.

- In the K20_100 MHz range the parts without FlexNVM memory have P-Flash swap feature, so you are looking for MK20DN512xxx10 part numbers.

I hope this helps.


Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply