Is MK22FN1M0AVLH12 pre-programmed with flashloader?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is MK22FN1M0AVLH12 pre-programmed with flashloader?

1,646件の閲覧回数
jennywang
Contributor I

I read through the forum, found a list of MCUs pre-programmed with flashloader which doen't  have MK22FN1M0AVLH12 listed. Doe Flashloader support this MCU now? What is in this IC's flash when it goes out from factory? If it's empty, can I order pre-programmed ICs with my bootloader ported from bootloader 1.2?

Thanks,

Jenny

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,505件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jenny,

The MK22FN1M0AVLH12 contains the Flashloader in the Flash from the factory as the Fig1 shows.

2016-04-14_9-23-41.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,505件の閲覧回数
jennywang
Contributor I

But From 3/2015's post, the K22_120 family doesn't include 1Mb version.  And from test, looks like the IC is empty. Please verify the flashloader support the particular IC MK22FN1M0AVLH12.

Jenny

flashloader.png

0 件の賞賛
返信