IrDA on FRDM KE06

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IrDA on FRDM KE06

1,543件の閲覧回数
pramodtm-b46240
Contributor III

Hi all,

     Does anyone have an example IrDA code on FRDM-KE06?

Thanks,

Pramod T M

ラベル(1)
0 件の賞賛
返信
1 返信

1,277件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

You may find useful this document that shows the implementation of the infrared on the UART0 using the FRDM-KE02Z platform.

Implementing infrared functions on UART0 with FRDM-KE02Z platform.

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------