IrDA on FRDM KE06

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IrDA on FRDM KE06

1,519 Views
pramodtm-b46240
Contributor III

Hi all,

     Does anyone have an example IrDA code on FRDM-KE06?

Thanks,

Pramod T M

Labels (1)
0 Kudos
Reply
1 Reply

1,253 Views
adriancano
NXP Employee
NXP Employee

Hi,

You may find useful this document that shows the implementation of the infrared on the UART0 using the FRDM-KE02Z platform.

Implementing infrared functions on UART0 with FRDM-KE02Z platform.

I hope this information can help you.

Regards,

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. It would be nice!

-----------------------------------------------------------------------------------------------------------------------