Interrupts on FRDM-KL25z using Keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupts on FRDM-KL25z using Keil

1,095 Views
User1675499243
Contributor I

I need a simple code to run interrupts on FRDM-KL25z using Keil.

0 Kudos
Reply
1 Reply

1,087 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You can download the sdk in this link 'mcuxpresso.nxp.com/en/select'. It has keil project.

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply