Interrupt numbers (Vector vs IRQ)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt numbers (Vector vs IRQ)

ソリューションへジャンプ
3,362件の閲覧回数
nijo
Contributor II

Hey,

 

I am working with the MK60N512VMD100.

 

I have a question about the Interrupt enumerations. In the header, MK60N512VMD100.h I notice that the PIT channels have iterrupt numbers 84, 85, 86 and 87.

 

/*! Interrupt Number Definitions */
typedef enum {

...

...

INT_PIT0 = 84, /*!< PIT timer channel 0 interrupt */
INT_PIT1 = 85, /*!< PIT timer channel 1 interrupt */
INT_PIT2 = 86, /*!< PIT timer channel 2 interrupt */
INT_PIT3 = 87, /*!< PIT timer channel 3 interrupt */

...

...

 

Which also correspond to the interrupt vector

 

static __declspec(vectortable) tVectorTable __vect_table = { 

...

...

(tIsrFunc)&isrINT_PIT0, /* 84 (0x00000150) (prior: 0) */
(tIsrFunc)&isrINT_PIT1, /* 85 (0x00000154) (prior: 0) */
(tIsrFunc)&isrINT_PIT2, /* 86 (0x00000158) (prior: 0) */
(tIsrFunc)&isrINT_PIT3, /* 87 (0x0000015C) (prior: 0) */

...

 

However, the "numbers" used to set the interrupt priorites are different. (Here I used the help tool in Code Warrior (Device Init.) 

 

/* Common initialization of the CPU registers */
/* NVICIP68: PRI68=0 */
NVICIP68 = (uint8_t)0x00U;
/* NVICIP69: PRI69=0 */
NVICIP69 = (uint8_t)0x00U;
/* NVICIP70: PRI70=0 */
NVICIP70 = (uint8_t)0x00U;
/* NVICIP71: PRI71=0 */
NVICIP71 = (uint8_t)0x00U;

 

It might be that I am missing something obvious here. But how does 68, 69, 70 and 71 correspond to  84, 85, 86 and 87. To me it seems like there is a 16 number offset.

 

Grateful for any help,

0 件の賞賛
返信
1 解決策
2,828件の閲覧回数
nijo
Contributor II

After checking the manual it seems there is an offset between the Vector and the IRQ that stems from the seperation between ARM core system handels and the non-core system handlers. This correspond exacly to my problem.

 

Attached for clearification.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,829件の閲覧回数
nijo
Contributor II

After checking the manual it seems there is an offset between the Vector and the IRQ that stems from the seperation between ARM core system handels and the non-core system handlers. This correspond exacly to my problem.

 

Attached for clearification.

0 件の賞賛
返信