Interrupt handler question for kinetisKE04 i2c driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt handler question for kinetisKE04 i2c driver

Jump to solution
3,186 Views
jun1
Contributor V

Thank you for all your help.

In the SDK_2_11_0_MKE04Z128xxx4 driver fsl_i2c.c there is the following interrupt handler.
Will something bad happen if I remove this last DSB instruction? On the contrary, what does it prevent?

static void I2C_TransferCommonIRQHandler(I2C_Type *base, void *handle)
{
  uint8_t tmpS = base->S;
  uint8_t tmpC1 = base->C1;

  /* Check if master interrupt. */
  if ((0U != (tmpC1 & I2C_C1_MST_MASK)) || (0U != (tmpS & (uint8_t)kI2C_ArbitrationLostFlag)))
  {
    s_i2cMasterIsr(base, handle);
  }
  else
  {
    s_i2cSlaveIsr(base, handle);
  }
  __DSB();
  }

}



Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,180 Views
bobpaddock
Senior Contributor IV

Far safer to leave it.  It assures that everything is completed before the interrupt exits.
Taking it out leaves the system open to 'once in a blue moon', hair pulling, kid of race condition crashes.

For M4 based processors is is required due to errata:

* // Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store
* // immediate overlapping exception return operation might vector
* // to incorrect interrupt

In theory is is not required on the M0(+) cores.
Rarely does theory work in the Real World...

/*
* Data Synchronization Barrier (DSB): Ensures that all explicit data
* memory transfer before the DSB are complete before any instruction
* after the DSB is executed.
*
* Ensure effects of an access to SCS take place before the next
* operation
*
* Ensure memory is updated before the next operation, for
* example, SVC, WFI, WFE.
*
* Vector table changes:
* If the program changes an entry in the vector table,
* and then enables the corresponding exception, a DSB
* instruction should be used between these two
* operations. This ensures that if the exception is
* taken after being enabled the processor uses the new
* exception vector. If the updated vector table is
* required immediately, for example if an SVC
* immediately follows an update to the SVC table entry
* via a store, then a DSB is also required.
*
* Memory Map modifications:
* If the system contains a memory map switching
* mechanism then use a DSB instruction after switching
* the memory map in the program. This ensures subsequent
* instruction execution uses the updated memory map, if
* the memory system makes the updated memory map visible
* to all subsequent memory accesses.
*
* Note:
* An ISB or an exception entry/return is required
* to ensure that the subsequent instructions are
* fetched using the new memory map.
*
* The memory barrier instructions, DMB and DSB, can be used to ensure
* that the write buffer on the processor has completed its operation
* before subsequent operations can be started. However, it does not
* check the status of the bus level write buffers. In such cases, if
* the system is based on AHB or AHB Lite, you might need to perform a
* dummy read through the bus bridge to ensure that the bus bridge has
* completed its operation.
*
* The Cortex-M0 processor (r0p0) and the Cortex-M0+ processor (r0p0)
* do not include a write buffer in their processor bus interface.
*
* Architecturally, a DSB instruction should be used after changing
* the VTOR if an exception is to be generated immediately and should
* use the latest vector table setting.
*
* In Cortex-M3, Cortex-M4 and Cortex-M0+ processors, accesses to the
* SCS have the DSB behavior, so there is no need to insert the DSB
* instruction.
*
* A DSB is required before generating self-reset to ensure all
* outstanding transfers are completed. The use of the CPSID I
* instruction is optional.
*/

// The code I use:
//The 'memory' clobber barrier prevents "code motion".

#define ATTR_NO_INSTRUMENT_FUNCTION __attribute__( ( no_instrument_function ) )

static inline ATTR_NO_INSTRUMENT_FUNCTION void sync_barrier_data( void )
{
__asm__ __volatile__ ("dsb");
__asm__ __volatile__ ("" ::: "memory");
}

View solution in original post

0 Kudos
Reply
2 Replies
3,168 Views
jun1
Contributor V

Thank you for your advice.


OK. Leave it as it is.


Also, I totally agree with the following words.

"Theory rarely works in the real world ..."

 

 

A good day

0 Kudos
Reply
3,181 Views
bobpaddock
Senior Contributor IV

Far safer to leave it.  It assures that everything is completed before the interrupt exits.
Taking it out leaves the system open to 'once in a blue moon', hair pulling, kid of race condition crashes.

For M4 based processors is is required due to errata:

* // Add for ARM errata 838869, affects Cortex-M4, Cortex-M4F Store
* // immediate overlapping exception return operation might vector
* // to incorrect interrupt

In theory is is not required on the M0(+) cores.
Rarely does theory work in the Real World...

/*
* Data Synchronization Barrier (DSB): Ensures that all explicit data
* memory transfer before the DSB are complete before any instruction
* after the DSB is executed.
*
* Ensure effects of an access to SCS take place before the next
* operation
*
* Ensure memory is updated before the next operation, for
* example, SVC, WFI, WFE.
*
* Vector table changes:
* If the program changes an entry in the vector table,
* and then enables the corresponding exception, a DSB
* instruction should be used between these two
* operations. This ensures that if the exception is
* taken after being enabled the processor uses the new
* exception vector. If the updated vector table is
* required immediately, for example if an SVC
* immediately follows an update to the SVC table entry
* via a store, then a DSB is also required.
*
* Memory Map modifications:
* If the system contains a memory map switching
* mechanism then use a DSB instruction after switching
* the memory map in the program. This ensures subsequent
* instruction execution uses the updated memory map, if
* the memory system makes the updated memory map visible
* to all subsequent memory accesses.
*
* Note:
* An ISB or an exception entry/return is required
* to ensure that the subsequent instructions are
* fetched using the new memory map.
*
* The memory barrier instructions, DMB and DSB, can be used to ensure
* that the write buffer on the processor has completed its operation
* before subsequent operations can be started. However, it does not
* check the status of the bus level write buffers. In such cases, if
* the system is based on AHB or AHB Lite, you might need to perform a
* dummy read through the bus bridge to ensure that the bus bridge has
* completed its operation.
*
* The Cortex-M0 processor (r0p0) and the Cortex-M0+ processor (r0p0)
* do not include a write buffer in their processor bus interface.
*
* Architecturally, a DSB instruction should be used after changing
* the VTOR if an exception is to be generated immediately and should
* use the latest vector table setting.
*
* In Cortex-M3, Cortex-M4 and Cortex-M0+ processors, accesses to the
* SCS have the DSB behavior, so there is no need to insert the DSB
* instruction.
*
* A DSB is required before generating self-reset to ensure all
* outstanding transfers are completed. The use of the CPSID I
* instruction is optional.
*/

// The code I use:
//The 'memory' clobber barrier prevents "code motion".

#define ATTR_NO_INSTRUMENT_FUNCTION __attribute__( ( no_instrument_function ) )

static inline ATTR_NO_INSTRUMENT_FUNCTION void sync_barrier_data( void )
{
__asm__ __volatile__ ("dsb");
__asm__ __volatile__ ("" ::: "memory");
}

0 Kudos
Reply