Interrupt does nothing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interrupt does nothing

ソリューションへジャンプ
2,716件の閲覧回数
javierhernande1
Contributor IV

Hello,

I have this code in order to print a message when the SW3 is pressed but enter in the IF conditional and not print the message and it does not go back into the loop.

I'm using McuExpresso and SDK2.5, the gpios are initialized from pin_mux.c and worsk fine with the numbers and letters in the 7 segment led display, but not the interrupt.

Should I initialize the interrupt also in pin_mux.c, instance of the source file? (as it's in the examples)

/* Init input switch GPIO.*/
#if (defined(FSL_FEATURE_PORT_HAS_NO_INTERRUPT) && FSL_FEATURE_PORT_HAS_NO_INTERRUPT)
 GPIO_SetPinInterruptConfig(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, kGPIO_InterruptFallingEdge);
#else
 PORT_SetPinInterruptConfig(BOARD_SW_PORT, BOARD_SW_GPIO_PIN, kPORT_InterruptFallingEdge);
#endif
 EnableIRQ(BOARD_SW_IRQ);
 GPIO_PinInit(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, &sw_config);‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Best regards

ラベル(1)
1 解決策
2,554件の閲覧回数
nxf51211
NXP Employee
NXP Employee

Hi Javier,

I checked both your main and pinmux files, and I noticed that you don't set SW3 completely. When I tried your code on my side, I saw that you have a function at pinmux.c that you never use called "BOARD_InitButtonsPins" where you can see the configuration for SW3; based on this observation I just added this function inside your main function and with this I was able to call the SW3 interruption without any problem.

int main(void) {
  /* Define the init structure for the input switch pin */
     gpio_pin_config_t sw_config = {
         kGPIO_DigitalInput, 0,
     };

   /* Init board hardware. */
    BOARD_InitBootPins();

    /**I added your function here!******************************************************/

    BOARD_InitButtonsPins();

    /*********************************************************************************/

    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
   /* Init FSL debug console. */
    BOARD_InitDebugConsole();

    PRINTF("Starting program!\n");

/* Init input switch GPIO.*/
#if (defined(FSL_FEATURE_PORT_HAS_NO_INTERRUPT) && FSL_FEATURE_PORT_HAS_NO_INTERRUPT)
 GPIO_SetPinInterruptConfig(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, kGPIO_InterruptFallingEdge);
#else
 PORT_SetPinInterruptConfig(BOARD_SW_PORT, BOARD_SW_GPIO_PIN, kPORT_InterruptFallingEdge);
#endif
 EnableIRQ(BOARD_SW_IRQ);
 GPIO_PinInit(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, &sw_config);


 while(1)
 {
  if(g_ButtonPress)
  {
   //for(int i = 0; i<8;i++)
   //{
    PRINTF("button pressed");
    //GPIO_PortToggle((void*)base[i], letter[4][i] << pin[i]);
    //PRINTF("Base %d, Pin %d\n",base[i],pin[i]);
    //delay();
    /* Reset state of button. */
    g_ButtonPress = false;
   //}
   //for (int i=0; i<8; i++){led[i] = number[4][i];}
  }
 }
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I hope this can help you.

Best Regards,

Ricardo Delsordo

元の投稿で解決策を見る

2 返答(返信)
2,555件の閲覧回数
nxf51211
NXP Employee
NXP Employee

Hi Javier,

I checked both your main and pinmux files, and I noticed that you don't set SW3 completely. When I tried your code on my side, I saw that you have a function at pinmux.c that you never use called "BOARD_InitButtonsPins" where you can see the configuration for SW3; based on this observation I just added this function inside your main function and with this I was able to call the SW3 interruption without any problem.

int main(void) {
  /* Define the init structure for the input switch pin */
     gpio_pin_config_t sw_config = {
         kGPIO_DigitalInput, 0,
     };

   /* Init board hardware. */
    BOARD_InitBootPins();

    /**I added your function here!******************************************************/

    BOARD_InitButtonsPins();

    /*********************************************************************************/

    BOARD_InitBootClocks();
    BOARD_InitBootPeripherals();
   /* Init FSL debug console. */
    BOARD_InitDebugConsole();

    PRINTF("Starting program!\n");

/* Init input switch GPIO.*/
#if (defined(FSL_FEATURE_PORT_HAS_NO_INTERRUPT) && FSL_FEATURE_PORT_HAS_NO_INTERRUPT)
 GPIO_SetPinInterruptConfig(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, kGPIO_InterruptFallingEdge);
#else
 PORT_SetPinInterruptConfig(BOARD_SW_PORT, BOARD_SW_GPIO_PIN, kPORT_InterruptFallingEdge);
#endif
 EnableIRQ(BOARD_SW_IRQ);
 GPIO_PinInit(BOARD_SW_GPIO, BOARD_SW_GPIO_PIN, &sw_config);


 while(1)
 {
  if(g_ButtonPress)
  {
   //for(int i = 0; i<8;i++)
   //{
    PRINTF("button pressed");
    //GPIO_PortToggle((void*)base[i], letter[4][i] << pin[i]);
    //PRINTF("Base %d, Pin %d\n",base[i],pin[i]);
    //delay();
    /* Reset state of button. */
    g_ButtonPress = false;
   //}
   //for (int i=0; i<8; i++){led[i] = number[4][i];}
  }
 }
}
‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

I hope this can help you.

Best Regards,

Ricardo Delsordo

2,554件の閲覧回数
javierhernande1
Contributor IV

Thank you, now works fine.

BR

0 件の賞賛
返信