Install OpenSDA on K64 (not K20)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install OpenSDA on K64 (not K20)

1,519 Views
roymessinger
Contributor V

Can I install the OpenSDA directly on the K64F component or must I place a K20 controller on-board as implemented on the FRDM-K64F board?

If so, any tutorials?

Thx

Tags (1)
0 Kudos
Reply
1 Reply

1,147 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Roy,

   The opensda is designed for the on board K20, not for K64 in the FRDM-K64, after the K20 have the opesda code, it will be the opensda debugger or JLINK debugger(with jlink firmware).

  So, please install the opensda on the K20 in the FRDM-K64, the on board opensda debugger can download the K64 code to the K64.

Wish it helps you!

If you still have any problem, please let us know.
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply