Inquiry Kinetis manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inquiry Kinetis manual

ソリューションへジャンプ
5,151件の閲覧回数
lim
Contributor II

Hi NXP

 

I found a Flash Security (FSEC)  register difference on manual

AN4507 - Kinetis manual

7      6            5      4           3         2          1    0 

KEYEN         MEEN           FSLACC          SEC

KEA64RM - KEA64RM manual

7         6            5     4       3    2                 1     0

KEYEN                 Reserved                       SEC

 

Can't we use a MEEN register on a KEA64RM ?

can i know which register is correct?

0 件の賞賛
返信
1 解決策
5,146件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
5,147件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
5,134件の閲覧回数
lim
Contributor II
I have an additional question.
 
 

AN4507 - Kinetis manual

Mass erase is disabled (MEEN 10)

 

I want use a mass erase disabled function on KEA64

but on KEA64RM MEEN is reserved , so we can't use that function on KEA64?

0 件の賞賛
返信
5,132件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Yeah, you are right

0 件の賞賛
返信
5,121件の閲覧回数
lim
Contributor II

Hi

 

Mass erase is disabled (MEEN 10)

 

Is there any other way to disable that function?

 

Thank you

0 件の賞賛
返信
5,111件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

May be you can refer the FPROT. It can protect the flash from programming and erasing.

nxf56274_0-1637115691200.pngnxf56274_0-1637115691200.png

 

BR,

Da

0 件の賞賛
返信
5,103件の閲覧回数
lim
Contributor II

Thank you 

if we enable the FPROT , mass erase is still working right? (JTAG)

 

0 件の賞賛
返信
5,091件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. You can also try to use the backdoor key to set the flash as security to avoid being erased.

0 件の賞賛
返信
5,138件の閲覧回数
lim
Contributor II

Thank you very mcuh.!

0 件の賞賛
返信