Inquiry Kinetis manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Inquiry Kinetis manual

跳至解决方案
3,496 次查看
lim
Contributor II

Hi NXP

 

I found a Flash Security (FSEC)  register difference on manual

AN4507 - Kinetis manual

7      6            5      4           3         2          1    0 

KEYEN         MEEN           FSLACC          SEC

KEA64RM - KEA64RM manual

7         6            5     4       3    2                 1     0

KEYEN                 Reserved                       SEC

 

Can't we use a MEEN register on a KEA64RM ?

can i know which register is correct?

0 项奖励
回复
1 解答
3,491 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
8 回复数
3,492 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,479 次查看
lim
Contributor II
I have an additional question.
 
 

AN4507 - Kinetis manual

Mass erase is disabled (MEEN 10)

 

I want use a mass erase disabled function on KEA64

but on KEA64RM MEEN is reserved , so we can't use that function on KEA64?

0 项奖励
回复
3,477 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Yeah, you are right

0 项奖励
回复
3,466 次查看
lim
Contributor II

Hi

 

Mass erase is disabled (MEEN 10)

 

Is there any other way to disable that function?

 

Thank you

0 项奖励
回复
3,456 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

May be you can refer the FPROT. It can protect the flash from programming and erasing.

nxf56274_0-1637115691200.png

 

BR,

Da

0 项奖励
回复
3,448 次查看
lim
Contributor II

Thank you 

if we enable the FPROT , mass erase is still working right? (JTAG)

 

0 项奖励
回复
3,436 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. You can also try to use the backdoor key to set the flash as security to avoid being erased.

0 项奖励
回复
3,483 次查看
lim
Contributor II

Thank you very mcuh.!

0 项奖励
回复