Inquiry Kinetis manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry Kinetis manual

Jump to solution
5,186 Views
lim
Contributor II

Hi NXP

 

I found a Flash Security (FSEC)  register difference on manual

AN4507 - Kinetis manual

7      6            5      4           3         2          1    0 

KEYEN         MEEN           FSLACC          SEC

KEA64RM - KEA64RM manual

7         6            5     4       3    2                 1     0

KEYEN                 Reserved                       SEC

 

Can't we use a MEEN register on a KEA64RM ?

can i know which register is correct?

0 Kudos
Reply
1 Solution
5,181 Views
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
8 Replies
5,182 Views
nxf56274
NXP Employee
NXP Employee

Hi,

 

The mcu RM is more accurate than the application note. So if the kea64 RM doesn't describe the bit, we shouldn't use it.

 

Have a great day,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
5,169 Views
lim
Contributor II
I have an additional question.
 
 

AN4507 - Kinetis manual

Mass erase is disabled (MEEN 10)

 

I want use a mass erase disabled function on KEA64

but on KEA64RM MEEN is reserved , so we can't use that function on KEA64?

0 Kudos
Reply
5,167 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Yeah, you are right

0 Kudos
Reply
5,156 Views
lim
Contributor II

Hi

 

Mass erase is disabled (MEEN 10)

 

Is there any other way to disable that function?

 

Thank you

0 Kudos
Reply
5,146 Views
nxf56274
NXP Employee
NXP Employee

Hi,

May be you can refer the FPROT. It can protect the flash from programming and erasing.

nxf56274_0-1637115691200.pngnxf56274_0-1637115691200.png

 

BR,

Da

0 Kudos
Reply
5,138 Views
lim
Contributor II

Thank you 

if we enable the FPROT , mass erase is still working right? (JTAG)

 

0 Kudos
Reply
5,126 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. You can also try to use the backdoor key to set the flash as security to avoid being erased.

0 Kudos
Reply
5,173 Views
lim
Contributor II

Thank you very mcuh.!

0 Kudos
Reply