Initial support for low-power in Linux on Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Initial support for low-power in Linux on Kinetis

1,021 次查看
vladimirkhusain
Contributor III

Emcraft has made available an initial implementation of low-power mode in Linux on the Kinetis K70 & K61 processors. Using the Linux "suspend-to-RAM" framework, the power consumption of the Kinetis running Linux (using the Emcraft System-On-Module as the hardware platform) goes down to as low as 600-700 uA while in suspend. Wake-up is instantenous on configured I/O events such as RTC alarm triggers or activity on UART RX.

Details available from: Linux Low-Power Mode on Kinetis

标记 (3)
0 项奖励
回复
0 回复数