Initial Programming of K66 with JTAGjet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Initial Programming of K66 with JTAGjet

1,525 Views
johnhannon
Contributor I

I am working with a custom board with a MK66FN2MOVMD18 processor.  Whenever I try to connec using JTAGjet I get the error "Fatal error:  Reading CPU status failed"

0 Kudos
Reply
1 Reply

1,382 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi John,

If it is possible, could you please post the K66 JTAG related circuit?

Or you could check chapter 2.1.5.3 Debug interface of <<Kinetis Peripheral Module Quick Reference>>.

If you have another debugger tool, such as Segger J-Link or P&E USB Multilink? If there with also the same result?

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply