Initial Programming of K66 with JTAGjet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Initial Programming of K66 with JTAGjet

1,523件の閲覧回数
johnhannon
Contributor I

I am working with a custom board with a MK66FN2MOVMD18 processor.  Whenever I try to connec using JTAGjet I get the error "Fatal error:  Reading CPU status failed"

0 件の賞賛
返信
1 返信

1,380件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi John,

If it is possible, could you please post the K66 JTAG related circuit?

Or you could check chapter 2.1.5.3 Debug interface of <<Kinetis Peripheral Module Quick Reference>>.

If you have another debugger tool, such as Segger J-Link or P&E USB Multilink? If there with also the same result?

Thank you for the attention.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信